Tariff Selection via the digital input


Tariff selection via the digital input

 

A switchover from one tariff to another can be performed via the digital input. Depending on the status of the input signal, tariff meter 1 or tariff meter 2 is used. Two of the four tariffs of the device can be used via the digital input.

Via the web server, you can manually configure up to four tariffs (identifiers 1...4) and read them via the communication interface.

 

Navigation on the web server

“Settings, Tariffs”

 

Menu: “Settings, Tariffs, Digital input”
Menu: “Settings, Tariffs, Digital input”

 

Status

The “Status” area shows the current status of the digital input.

Settings

Set the impulse counter according to your requirements.

Identifier

Define the two identifiers (names) for your tariffs.

Mode

Specify the digital input as method for using the tariff selection.

Digital input

Define the status of the digital input in relation to the identifier.

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history